Define Derived Parameter
Derived parameters provides the option to define the parameters using expressions based on the use case scenarios.
Perform the following steps to define derived parameters:
-
Click Parameter > Derived tab.
When adding a record for any parameter under the Parameter section (Constructional, Operational, Derived, Predicted, or Physical Property), if a parameter is already associated with any of these categories, it does not appear in the add record parameter list. For example, if you add a record for a Constructional parameter, the same parameter is not available for selection in Constructional or any other listed categories.
-
Click Add Record button.
-
Select the Derived parameters required for this template by selecting the check box next to them.
You can also search the required parameters using the search box in the top right corner of the window.
Ensure the derived parameters added doesn’t have a interdependency on each other to avoid cyclic dependency error.
-
Click Add.
-
In Derived tab after adding the parameter, click Define button in the Formula column. Expression Builder window opens.
APM application enables you to define derived parameters by providing mathematical expression based on constructional, operational or other derived parameters of the same template. You can define derived parameters using mathematical expression at the template level. When you instantiate the template and create specific equipment instance, you can specify further details for the derived parameter calculation such as calculation frequency, OT tags to be used for calculation etc.
-
Enter the details to define the derived parameter. Following table provides description of the fields and options in Expression Builder window.
Field
Description/Action
Name
Enter a unique name for the Expression.
Description
Enter short description of the Expression.
Keyword
Enter a Keyword.
Expression
Define an expression/formula to derive the parameter from other parameters and functions.
Input Variable
Input Variable helps in building an expression using values from different parameter categories, namely Constructional, Operational, Derived, Predicted, Reference, and Physical Property.
Functions
-
Click the tab to view the options. Various functions are grouped under three categories, namely Trigonometry, Logarithmic, Mathematical and Aggregation.
-
Click a category to view the functions under them.
-
Click a function to use it in the expression. The function appears in the Expression field.
You can also use the search box on the top of the tab to search a function to use it in a expression.
Parameters
-
Click the tab to view the options. All the parameters are grouped under five categories, namely Constructional, Operational, Derived, Predicted, and Reference.
-
Click a category to view the parameters under them.
-
Click a parameter you want to use it in the expression. Select the nature of the parameter from the options displayed. The function appears in the Expression field.
You can also use the search box on the top of the tab to search a Parameters to use it in a expression.
Operators
-
Click the tab to view the options.
-
Click Mathematical, Comparison, Logical and Conditional Operators to view the Operators under them.
-
Click an Operator to use it in the expression. The Operator appears in the Expression field.
You can also use the search box on the top of the tab to search an Operator to use it in a expression.
Constants
-
Click the tab to view the available constants.
-
Click a Constant to use it in the expression. The Constant appears in the Expression field.
You can also use the search box on the top of the tab to search a constant to use it in a expression.
Expression Builder
For more information about Expression Builder, Functions, Operators, Expression Grammar, and Constants, see section Calculation Engine.
-
-
Click Validate button to validate the Expression created. "Successfully validated" message should appear at the bottom of the window.
-
Click Save.